Position Encoder Resolution (Motor Revolution)
Index.Sub | |
Data Type | Unsigned32 |
Access | Read/Write |
PDO Mappable | No |
Unit | -- |
Range |
1 - Unsigned32 |
Default Value | 1 |
Store Supported | Yes |
Description |
The Position Encoder Resolution defines the ratio of encoder increments per motor revolutions :
|
Notes |
See Factor Group. |